cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f205vbt6

Juan1
Associate
I need to program the stm32f205vbt6, which programmer do you recommend? Why does st-link v2 Chinese version not recognize it?
1 REPLY 1
TDK
Guru

> I need to program the stm32f205vbt6, which programmer do you recommend?

Any official programmer will work. Perhaps STLINK-V3MINIE which is cheap.

> Why does st-link v2 Chinese version not recognize it?

A few things could be going on.

  • Perhaps board isn't powered, is wired correctly, or has some other hardware error.
  • Perhaps the programmer is broken and doesn't work, in which case you should ask whoever sold it to you.

Does STM32CubeProgrammer recognize the programmer at all? Screenshots and error messages help to describe the problem accurately.

If you feel a post has answered your question, please click "Accept as Solution".