2013-07-22 05:37 AM
Hi everyone,
is it possible to enter the bootmode without setting the Boot0/1-pins with an external switch?2013-07-22 05:44 AM
is it possible to enter the bootmode without setting the Boot0/1-pins with an external switch?
Yes, you can change the zero mapping, and you can also jump to it.2013-07-22 06:08 AM
What you mean with Zero-Mapping?
2013-07-22 06:51 AM
One of the primary roles of the BOOT0/1 pins is to define what memory (FLASH, ROM, RAM) is mapped/shadowed at address zero.
ie FLASH at 0x00000000 and 0x08000000, the Cortex-M3 expects the boot memory to be at zero.