2007-12-20 09:43 AM
STM32F10xxx USB developer kit
2011-05-17 03:20 AM
Hi all!
I'm very new on ARM and USB program. I'm trying to run the Mass_Storage demo code of the STM32F10xxx USB developer kit but the the following loop never ends. /* Wait until device is configured */ while (pInformation->Current_Configuration == 0) { NOP_Process(); } I'm using CrossWorks V1.7 and a home made board with a 103RBT6 clocked at 10MHz. All others demos of the firmware library works good so I think my board is OK. Thank you for any help. Maia (from Brazil).2011-05-17 03:20 AM
Problem solved. Changed the cristal to 9 MHz and configured PLL to X8. Now running at 72 MHZ.
:-D2011-05-17 03:20 AM
Hi,
I'm searching the USB developer kit download, where can I find this?
Cheers,
Sven
2011-05-17 03:20 AM
Hi Maia,
Well Done, To run USB on STM32 performance line you need to configure the CPU at a fixed frequency of 72Mhz or 48Mhz because the USB analog cell needs the 48MHz for the Physical layer and Protocol compliancy with USB2.0 Full Speed :-) Regards, STOne32