Question
STM32f10x WWDG ''Window WatchDog Timer''
Posted on January 21, 2014 at 13:46
Hello
I am using STM32f103RET6 in my project. This project is very important and device should never stop working. Also device is remote and it is not possible to reset it easily. I try to use WWDG for unforeseen cpu faults. The problem is that I use 1sec delay loop in my project and the MAX timeout time for WWDG is about 58ms. When I use it in my project device reset before one loop running. Any suggestion to solve this problem in my project? Regards, Thanks,