stm32f10x eeprom emulation
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-28 6:51 PM
Posted on December 29, 2015 at 03:51
Hello, i gone through AN2954 and to make it simple,
i just get out the eeprom write & read (don't am i correct to do so) EEprom write: uint16_t EE_WriteVariable(uint16_t VirtAddress, uint16_t Data) { uint16_t Status = 0; /* Write the variable virtual address and value in the EEPROM */ Status = EE_VerifyPageFullWriteVariable(VirtAddress, Data); /* In case the EEPROM active page is full */ if (Status == PAGE_FULL) { /* Perform Page transfer */ Status = EE_PageTransfer(VirtAddress, Data); } /* Return last operation status */ return Status; } //=================== EEPROM READ uint32_t EEPROM_Read(uint16_t Address) { uint32_t readValue; FLASH_Unlock(); // Address = BANK1_WRITE_START_ADDR; readValue = (*(__IO uint16_t*) Address); FLASH_Lock(); return readValue; } However, when i process to do EE_WriteVariable(200, 14); FLASH_Unlock(); test_3 = EEPROM_Read(200); i cannot get the correct value in test_3. Can anyone help? Thanks
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-28 9:05 PM
Posted on December 29, 2015 at 06:05
Can anyone help?
Look, it's a 32-bit processor, you can't take a 16-bit variable and cast it into an address and expect it to function properly. You'll need to use the EEPROM abstraction to go retrieve your value, I don't think it exists at some linear memory address.
Tips, Buy me a coffee, or three.. PayPal Venmo
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
‎2015-12-28 10:17 PM
Posted on December 29, 2015 at 07:17 Thanks clive, can you explain more as i am new to 32bit world. what i do is take the core out from the following uint16_t EE_ReadVariable(uint16_t VirtAddress, uint16_t* Data); uint16_t EE_WriteVariable(uint16_t VirtAddress, uint16_t Data); and in the readvariable function //========= uint16_t EE_ReadVariable(uint16_t VirtAddress, uint16_t* Data) { uint16_t ValidPage = PAGE0; uint16_t AddressValue = 0x5555, ReadStatus = 1; uint32_t Address = 0x08010000, PageStartAddress = 0x08010000; /* Get active Page for read operation */ ValidPage = EE_FindValidPage(READ_FROM_VALID_PAGE); /* Check if there is no valid page */ if (ValidPage == NO_VALID_PAGE) { return NO_VALID_PAGE; } /* Get the valid Page start Address */ PageStartAddress = (uint32_t)(EEPROM_START_ADDRESS + (uint32_t)(ValidPage * PAGE_SIZE)); /* Get the valid Page end Address */ Address = (uint32_t)((EEPROM_START_ADDRESS - 2) + (uint32_t)((1 + ValidPage) * PAGE_SIZE)); /* Check each active page address starting from end */ while (Address > (PageStartAddress + 2)) { /* Get the current location content to be compared with virtual address */ AddressValue = (*(__IO uint16_t*)Address); /* Compare the read address with the virtual address */ if (AddressValue == VirtAddress) { /* Get content of Address-2 which is variable value */ *Data = (*(__IO uint16_t*)(Address - 2)); /* In case variable value is read, reset ReadStatus flag */ ReadStatus = 0; break; } else { /* Next address location */ Address = Address - 4; } } /* Return ReadStatus value: (0: variable exist, 1: variable doesn't exist) */ return ReadStatus; } and i just take this out /* Get content of Address-2 which is variable value */ *Data = (*(__IO uint16_t*)(Address - 2)); //========= i search from internet but no example show the eeprom read. it would be great if someone help. Thanks Jeff