2013-09-25 6:35 AM
Hi, I would like to use with Ethernet. I need to build minimal board. In datasheet I found: ''Ethernet MAC interface with dedicated DMA and IEEE 1588 support''. Is possible to connect RJ45 connector directly to MCU or I must add any other electronics parts?
Is good choice to use Ethernet in MCU or is better to buyhttps://www.olimex.com/Products/Modules/Ethernet/ENC28J60-H/
? How compilicated is minimal circuit with STM32 and Ethernet? Now I am using 8bit Arduino with ENC28J60 and board is very simple (http://www.instructables.com/id/A-credit-card-sized-Ethernet-Arduino-compatable-co/?ALLSTEPS
). Thank you for help!2013-09-25 6:53 AM
How good are your design/implementation skills?
You will need a PHY and RJ45 with suitable magnetics. See Pg 18http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00246066.pdf
If you want a lower cost implementation that supports 100 Mbps rather than just 10 Mbps, you'd go with the MAC integrated into the STM32, wouldn't you?2013-09-25 9:28 AM
My design skills are not very good :(
I am trying to build temperature watchdog with internet control. I need 1 input for 1-Wire temperature sensor, 2 outputs for relay and Ethernet interface. I do not need hight speed Ethernet, 10Mbps is sufficient. What MCU you recommend to me? I found and it looks good for me. What is your opinion? So I need only MCU, 25MHz crystal, RJ45 to MCU separator (for examplehttp://cz.farnell.com/pulse/h1012nl/module-transformer-ethernet/dp/2113972
) and +3.3V power supply. Is it all?2013-09-25 4:48 PM