cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F105RC DFU troubles

urasinov
Associate II
Posted on May 12, 2012 at 11:35

I have two board on STM32F105RCT6.

Both have same troubles.

I run board in bootloader mode.

I sure that MCU is in boot mode, because my programm doesn't work at this time.

I connect USB cable, windows can not recognize usb device (VID=0, PID=0).

Disconnect cable and connect at second time, again unknown device.

Reconnect at third time all is, windows recognize ''STM Device in DFU Mode''

I test two boards with different usb cables, on different PCs with WinXP and Win7.

I test it more than 20 times.

Alway windows recognize only at third connection.

Always first and seconds connections fail. Third, fourth and all other follow-up connections are ok.

I make pauses between connection from 1 sec to 30 seconds, Alwayw third connection is OK.

What happens?

MCU data code is 127.
0 REPLIES 0