2014-06-23 6:35 AM
I have problem with jump to application by bootloader.
The device used is the STM32F105R8. The bootloader does not jump in the application,it crashes in the function ''Jump_To_Application()''. The code of the bootloader making the jump is: #define APPLICATIONADDRESS (uint32_t)0x08008000 /* Test if user code is programmed starting from address ''ApplicationAddress'' */ if (((*(__IO uint32_t*)APPLICATIONADDRESS) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ JumpAddress = *(__IO uint32_t*) (APPLICATIONADDRESS + 4); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) APPLICATIONADDRESS); Jump_To_Application(); } In the application i have relocate the vector table: int main(void) { // __disable_irq(); /* Set the Vector Table base location at 0x8000 */ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8000); // __enable_irq(); /***************** Add your application code here ***************************/ ........ } I attached the image (bootloader + application) downloaded from flash.2014-06-25 6:07 AM
Awesome, I hope this all works out for you, but the presented facts appear internally inconsistent.
2014-06-26 12:06 AM
Look the ''stsw-stm32121_USB\STM32_USB-FS-Device_Lib_V4.0.0\Projects\Device_Firmware_Upgrade\binary_template'' use same method.
Bootloader ==> 0x08000000 to 0x08003000 Application ==> 0x08003000 to 0x08020000 In the main function set the Vector Table base location at 0x3000: NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x3000); The option target for application is:2014-06-26 5:03 AM
Look the ''stsw-stm32121_USB\STM32_USB-FS-Device_Lib_V4.0.0\Projects\Device_Firmware_Upgrade\binary_template'' use same method.
Bootloader ==> 0x08000000 to 0x08003000
Application ==> 0x08003000 to 0x08020000
In the main function set the Vector Table base location at 0x3000:
NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x3000);
Previously: The VECT_TAB_OFFSET must be equal 0x7000 ( 0x8000 - offset) else not function! So 0x7000 when it's 0x8000 is consistent with this? 64K-0x8000 = 0x9000! And the binary generated with a ResetHandler at ~0x08007000 when the linker is set at 0x08008000
2014-06-27 12:19 AM
I agree with
you!
This is the only
method
that works!
I asked
clarifications
the
ST
support
,
but
do not respond
!
2014-06-27 12:30 AM
I've got quite a lot of mileage on these types of solutions (boot loader + app, STM32), if it misbehaves in the manner you describe the problem is most likely in the project (options/metadata), the files it actually uses (paths, defines, pre-processor), and the tool chain (linker).
Keil support might be a better avenue. For ST you'd probably want to go via your local distributor and their FAE's, and have them thoroughly replicate and understand your issue.