cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103ZE Timer/ADC/PLL/ISR configuration help

madhu13
Associate III
Posted on August 11, 2010 at 13:01

STM32F103ZE Timer/ADC/PLL/ISR configuration help

5 REPLIES 5
kashif
Associate II
Posted on May 17, 2011 at 14:01

you are working on which IDE? generally IDE's have some example codes for different peripherals. try to run those examples.

you can download different helping material, manuals and sample codes from this link 

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110

hope this helps

madhu13
Associate III
Posted on May 17, 2011 at 14:01

thanks kashif87 for ur reply

i am using Keil uVision4 IDE...i saw the link but i didn't get any sample code there.. and m using STM32F103R8T6 controller.

madhu13
Associate III
Posted on May 17, 2011 at 14:01

i got an example of timer for Timer1 that worked well both in polling and interrupt methods. but now i am trying to configure Timer in the same way as bellow, i am using Keil IDE interrupt is not comming can you tell me what is the problem in this code...

main()

{

 RCC->APB1ENR=0x00000001; //Timer2 peripheral clock enable

 TIM2->PSC=0x0001;

 TIM2->ARR=0xffff;    //Autoreload value

 TIM2->CNT=0x0000;

 TIM2->EGR=0x0000; //0x0001;

 TIM2->CR1=0X0280;    //0x0281;//Prescalar is 10 ie. tDTS=4*tCK_INT, autoreload enabled

 TIM2->DIER = 0x0001;                        // enable interrupt

 NVIC->ISER[0]|= (1 << (TIM2_IRQChannel & 0x1F));

 //NVIC->ISER[0]=0x10000000;

 TIM2->CR1|=0X0001; 

 while(1)

 {;

 }

}

void TIM2_IRQhandler(void)

{

 if ((TIM2->SR & 0x0001) != 0)

  {

   i=~i;

   GPIOA->ODR=i;

  TIM2->SR=0x0000;

  //TIM2->CR1|=0X0001;

 }

}

   

Posted on May 17, 2011 at 14:01

Perhaps you should be initializing GPIO(A), the clocks for it and the port direction, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
madhu13
Associate III
Posted on May 17, 2011 at 14:01

ya i configured GPIOA as output push-pull and checked the o/p on logic analyzer window....its working fine now