2011-10-31 10:54 AM
HI!
I have a problem
with the following code
..
After
a few hours to
several days
.The maximum
was
to
14 days
Data
transmission
stops working
.Receive and transmit
works
in
one task
. (BACNET protocol)For
DMA
uses internal
RAM
.Receive
a
nd
other
tasks
work
sfurther
.
void USART3_SendData(unsigned char buffer[], int Len) {
if (Len > 500) { Len = 500; } memcpy(TxBuffer3Out, buffer, Len); DMA_InitTypeDef DMA_InitStructure5; DMA_DeInit(DMA1_Channel2); DMA_InitStructure5.DMA_PeripheralBaseAddr = USART3_DR_Base; DMA_InitStructure5.DMA_MemoryBaseAddr = TxBuffer3Out; DMA_InitStructure5.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure5.DMA_BufferSize = Len; DMA_InitStructure5.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure5.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure5.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure5.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure5.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure5.DMA_Priority = DMA_Priority_Low; DMA_InitStructure5.DMA_M2M = DMA_M2M_Disable; DMA_ITConfig(DMA1_Channel2, DMA_IT_TC, ENABLE); DMA_ITConfig(DMA1_Channel2, DMA_IT_TE, ENABLE); DMA_Init(DMA1_Channel2, &DMA_InitStructure5); USART_DMACmd(USART3, USART_DMAReq_Tx, ENABLE); DMA_ClearFlag(DMA1_FLAG_TC2); NVIC_EnableIRQ(DMA1_Channel2_IRQn); RS485_rts_enable(true); DMA1_Channel2->CCR |= DMA_CCR2_EN; OS_FlagID flag; start: flag = CoWaitForSingleFlag(USART3txFlag, 500); if (flag != E_OK && flag != E_TIMEOUT) { goto start; } CoTimeDelay(0, 0, 0, 20); RS485_rts_enable(false); }void DMA1_Channel2_IRQHandler(void) {//USART3 TX
if (DMA_GetITStatus(DMA1_IT_HT2) == SET) { DMA_ClearITPendingBit(DMA1_IT_HT2); } else if (DMA_GetITStatus(DMA1_IT_TC2) == SET) { DMA_ClearITPendingBit(DMA1_IT_TC2); USART_ITConfig(USART3, USART_IT_TC, ENABLE); } else if (DMA_GetITStatus(DMA1_IT_TE2) == SET) { DMA_ClearITPendingBit(DMA1_IT_TE2); } return; }void USART3_IRQHandler(void) {
if (USART_GetITStatus(USART3, USART_IT_TC) == SET) { USART_ClearITPendingBit(USART3, USART_IT_TC); USART_ITConfig(USART3, USART_IT_TC, DISABLE); CoEnterISR(); isr_SetFlag(USART3txFlag); CoExitISR(); return; }}
Any
idea
??Thanks!!
ArSi2011-10-31 5:37 PM
I'm unsure of the wisdom of constantly enabling/disabling interrupts, especially the USART TC one. And the point of having DMA interrupts if you're not actually doing anything with them.
I guess I'd attack this keeping the USART TC interrupt enabled, because it will always trail the DMA completion, and use it to progress the USART DMA to the next. Consider a method of chaining the pending data so it can transition more seamlessly between blocks of DMA'd data. Is all data on the USART sent via DMA? In terms of debugging the current code, and the failures, you'll need to examine what's not getting signalled, and looking at the USART and DMA registers in the failing condition to see if they are indicative of anything. For example the USART is holding an error state precluding further rx/tx operation until cleared. DMA can be very fussy about sequencing.2011-11-01 2:46 AM
The
same code
I have
used for
usart1
,usart2
.This
is
just
a
RS232
,problem does not occur
.Quantity
of data
is
transmitted
mainly through
usart1
significantly larger
.When it comes to
DMA
error
flag
was
there
so I
included
the command
to
restart
the processor
, butdid not come
.Data
sent
completely
and
without problems.
Debugger
I
was
hanging
there
already
3 days
,but as
it happens
error
had not occurred
.Most
annoying
,there are
lots
of
complex
code.
And it
works.
And
does not
thing
which should
run without
problems
2011-11-01 7:03 AM
there are
lots
of
complex
code.
Indeed, perhaps overly so, I'd be worried about your race condition and priority inversion problems, based on the code fragment presented.