Question
SPI Configuration
Posted on November 01, 2011 at 16:38
Hello,
I was learning reading the SPI documentation and there is something I do not understand. In the file stm32f10x_spi.h it is defined: #define SPI_Direction_2Lines_FullDuplex ((uint16_t)0x0000) #define SPI_Direction_2Lines_RxOnly ((uint16_t)0x0400) #define SPI_Direction_1Line_Rx ((uint16_t)0x8000) #define SPI_Direction_1Line_Tx ((uint16_t)0xC000) ... the four modalities for the SPI. The one I do not understand how the SPI_Direction_2Lines_RxOnly works. Can anybody explain me how to connect the wires (i.e. MISO, MOSI) between the slave and the master and how the flow of data work? Thanks in advance,