cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103vet6 no osc no cap Swd download ok

st128
Associate

 no osc no resist no osc but it run and download with swd light led pb12 ,but when fixed pin anybody know 

67C5C88B-4C82-4A2F-A99C-F5919B6B3DFC.jpeg

1496A3E0-41E3-4B6D-8C67-F9462D889761.jpeg

  • v2.9.0                  
          -------------------------------------------------------------------
    
    ST-LINK SN  : 16004A002933353739303541
    ST-LINK FW  : V2J38S7
    Board       : --
    Voltage     : 3.17V
    SWD freq    : 4000 KHz
    Connect mode: Under Reset
    Reset mode  : Hardware reset
    Device ID   : 0x414
    Revision ID : Rev X
    Device name : STM32F101/F103 High-density
    Flash size  : 512 KBytes
    Device type : MCU
    Device CPU  : Cortex-M3
    BL Version  : --
    
    
    
    Memory Programming ...
    Opening and parsing file: BlinkSTM32FC8.ino.bin
      File          : BlinkSTM32FC8.ino.bin
      Size          : 12944 Bytes
      Address       : 0x08000000 
    
    
    Erasing memory corresponding to segment 0:
    Erasing internal memory sectors [0 6]
    Download in Progress:
    
    
    File download complete
    Time elapsed during download operation: 00:00:00.774
    
    RUNNING Program ... 
      Address:      : 0x8000000
    Application is running, Please Hold on...
    Start operation achieved successfully
1 ACCEPTED SOLUTION

Accepted Solutions
STOne-32
ST Employee

Dear @st128 ,

 

Welcome in STCommunity !  and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note 

Getting started with STM32F10xxx hardware development - undefined

Hope it helps you.

STOne-32.

View solution in original post

2 REPLIES 2
STOne-32
ST Employee

Dear @st128 ,

 

Welcome in STCommunity !  and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note 

Getting started with STM32F10xxx hardware development - undefined

Hope it helps you.

STOne-32.

o,thank you