cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103VC and external SRAM

jonas2399
Associate II
Posted on March 29, 2010 at 14:20

STM32F103VC and external SRAM

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
jonas2399
Associate II
Posted on May 17, 2011 at 13:45

Also, I should have mentioned that I want to use FSMC.

Posted on May 17, 2011 at 13:45

This isn't a multiplexed device?

http://www.issi.com/pdf/61-64WV51216.pdf

You'd need to set the STM32 up for PSRAM, with the byte lanes.

Check the schematics provided for the STM3210E board

http://www.st.com/stonline/books/pdf/docs/14220.pdf

-Clive
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jonas2399
Associate II
Posted on May 17, 2011 at 13:45

Thanks for your answer. 

The evaluation board is based around the STM32F103ZET6 which has a lot more pins than mine, and therefore don't  need the addres/data multiplexing. 

The problem is that mine does not have enough pins for the adress bus, only eight. 

So the question really is: How do I connect an external SRAM to the STM32F103VC, which does not have enough pins for the entire SRAM adress bus, using FSMC?