cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103T8U6 compatibility

gmarocco
Associate
Posted on September 21, 2010 at 15:46

Is STM32VLDISCOVERY suitable for programming/debugging external STM32F103T8U6 (using serial wire debug port)? In order to program/debug STM32F103T8U6 in which way should JTDI,JTDO,JNTRST be connected?

1 REPLY 1
infoinfo968
Associate II
Posted on September 21, 2010 at 21:19

Yes. If you look at the User Manual (Document 17217, on the main STM32VLDiscovery page) it talks about this on pages 9 through 11. This references another document UM0627.

It says it is ''restricted to STM32F devices'' so presumably the one you list will work :)