cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103RG

bertuccimassimo
Associate
Posted on January 29, 2014 at 10:33

hallo, to program the STM32 microcontroller of my EVALST7590T-2 as base node or service node i can use the STMLINK and if i must to connect on STM32 UART SERVICE or on STM32 SWD ? And then what must i do? thanks. ST visual programmer is right for do it? thanks

#stm32f103rg
2 REPLIES 2
Posted on January 29, 2014 at 17:49

http://www.st.com/web/en/catalog/tools/PF255284

http://www.st.com/web/en/resource/technical/document/data_brief/DM00068323.pdf

Yeah, I'd probably us an ST-LINK connected to the SWD(JTAG), and then use the ST-LINK Utilities to blow in a .BIN or .HEX firmware image. This would be far the easiest route.

Alternatively the Serial connection with BOOT0 (UP_PROG jumper) settings should work with the

http://www.st.com/web/en/catalog/tools/PF257525

. To use the serial connector you'd need a USB-to-CMOS Serial adapter, not an RS232 Serial adapter/cable
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bertuccimassimo
Associate
Posted on February 10, 2014 at 12:38

thank you, my EVALST7590T-2 with STM32F103RG as default have firmware with base node or service node?