cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103RB + 3 ADC Channels + DMA

michaelsauer9
Associate II
Posted on October 28, 2014 at 11:16

Hi,

ive used the forum search before but i cannot find any thread that fits to my problem.

I tried to read out continiously 3 ADC channels from my sound filter electronics.

I already got values but the values are so ... i dont know.. wrong!? That is not possible to use them. First i thought it relies on my electronics but i tested the output or the input of noises with an oscilloscope but it was a clear gnd line, so i dont think that its the electronic part any more. 

I got on no sound playing such values:   Channel 1=1590 || 2=1279 || 3=4058

The are different if i play some sound but shouldnt be the values around zero if no sound would be played?

I attached my i hope well documented ADC library, maybe there is an simple issue i overread in the ''small'' datasheet :)

Greets

Michael

#adc #stm32f1 #dma
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0