cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 (Blue Pill) CAN BUS Communication

Javier Parra
Associate II

Hi,

I´m trying to communicate two blue pills between them using CAN bus, but when I try to run it, it doesn´t even finish the start up, because I tried to use a blink program selecting the CAN in the .ioc and not using it and doesn´t work.

Does anyone knows why does this happen?

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Peter BENSCH
ST Employee

I just stumbled across this thread because, like many others, it deals with the Bluepill. For a long time now, only clones and counterfeits have been used on it, which can flash an LED but do not (cannot) support many other peripheral functions. I now strongly suspect that there is also a counterfeit on your Bluepill.

Are you 100% sure that it is an original STM32F103?

Please check websites like e.g. hackaday.io or eevblog.com.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peter BENSCH
ST Employee

The so-called Blue Pill use illegally cloned STM32F103. ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.