2023-02-02 2:50 AM
Hi
I try to run SPI 1 on STM32F103C8 but when i send data i have only SCK signal. MOSI(PB5) is in high state (dont change).
SPI2 on PORTA works grate.
void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
LL_GPIO_AF_Remap_SWJ_NOJTAG();
while((AFIO->MAPR & AFIO_MAPR_SWJ_CFG_JTAGDISABLE) != AFIO_MAPR_SWJ_CFG_JTAGDISABLE);
/* USER CODE END SPI1_Init 2 */
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(spiHandle->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* SPI1 clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI1 GPIO Configuration
PB3 ------> SPI1_SCK
PB4 ------> SPI1_MISO
PB5 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
__HAL_AFIO_REMAP_SPI1_ENABLE();
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
for (uint16_t x=0; x<254; x++){
uint8_t chr = 0x55;
HAL_SPI_Transmit(&hspi1, &chr, 1, 1);
HAL_Delay(10);
HAL_GPIO_WritePin(PORT_LD, PIN_LD, SET);
HAL_Delay(1);
HAL_GPIO_WritePin(PORT_LD, PIN_LD, RESET);
HAL_Delay(1);
}
2023-02-02 5:39 AM
> __HAL_AFIO_REMAP_SPI1_ENABLE();
You need to enable AFIO clock in RCC for this to work.
JW
2023-02-02 5:57 AM
__HAL_AFIO_REMAP_SPI1_ENABLE(); is enable by HAL
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
__HAL_AFIO_REMAP_SPI1_ENABLE();
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
2023-02-02 6:16 AM
Try a simple program, which sets PB5 as a GPIO output and toggle it in program.
(In other words, check if PB5 is properly connected).
JW
2023-02-02 6:37 AM
Yes I check this at first time.
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_5, RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_5, SET);
works ok (whene SPI1 is disabled)
I also replase MCU to new one.
2023-02-02 2:19 PM
Ok
I found out what is causing the problem.
you can't have I2C1 enabled with SPI1 even if I2C1 pins are remapped
any way to bypass this problem?
2023-02-03 2:03 AM
> any way to bypass this problem?
Probably not in an easy way.
If you use I2C as master, you can try to bit-bang it.
You can consider using a different pin-compatible STM32.
JW