2014-09-26 2:18 AM
Hi Guys,
Im currently try to implement a USB. The programm isderived
from the CDC example. It is already working with 3 enpoint like in the CDC example. But I want only to work with 2 endpoint but when I configured it I get always a set configuration error when a want to communicate with the stm here a the configuration with 3 endpoints: usb_desc.cconst
uint8_t Virtual_Com_Port_DeviceDescriptor[] =
{
0x12,
/* bLength */
USB_DEVICE_DESCRIPTOR_TYPE,
/* bDescriptorType */
0x00,
0x02,
/* bcdUSB = 2.00 */
0xff,
/* Class: Vendor specific */
0x00,
/* bDeviceSubClass */
0x00,
/* bDeviceProtocol */
0x40,
/* bMaxPacketSize0 */
0x83,
0x04,
/* idVendor = 0x0483 */
0x01,
0xf0,
/* idProduct = 0xf001 */
0x00,
0x01,
/* bcdDevice = 2.00 */
1,
/* Index of string descriptor describing manufacturer */
2,
/* Index of string descriptor describing product */
3,
/* Index of string descriptor describing the device's serial number */
0x01
/* bNumConfigurations */
};
const
uint8_t Virtual_Com_Port_ConfigDescriptor[] =
{
/*Configuation Descriptor*/
0x09,
/* bLength: Configuation Descriptor size */
USB_CONFIGURATION_DESCRIPTOR_TYPE,
/* bDescriptorType: Configuration */
VIRTUAL_COM_PORT_SIZ_CONFIG_DESC,
/* wTotalLength:no of returned bytes */
0x00,
0x01,
/* bNumInterfaces: 1 interface */
0x01,
/* bConfigurationValue: Configuration value */
0x00,
/* iConfiguration: Index of string descriptor describing the configuration */
0x80,
/* bmAttributes: Bus powered */
500/2,
/* MaxPower 0 mA */
/*Data class interface descriptor*/
0x09,
/* bLength: Endpoint Descriptor size */
USB_INTERFACE_DESCRIPTOR_TYPE,
/* bDescriptorType: */
0x00,
/* bInterfaceNumber: Number of Interface */
0x00,
/* bAlternateSetting: Alternate setting */
0x03,
/* bNumEndpoints: 3 endpoints used */
0xff,
/* bInterfaceClass: ??? */
0x00,
/* bInterfaceSubClass: */
0x00,
/* bInterfaceProtocol: */
0x00,
/* iInterface: */
/*Endpoint 1 Descriptor*/
0x07,
/* bLength: Endpoint Descriptor size */
USB_ENDPOINT_DESCRIPTOR_TYPE,
/* bDescriptorType: Endpoint */
0x81,
/* bEndpointAddress: (IN1) */
0x02,
/* bmAttributes: Bulk */
VIRTUAL_COM_PORT_DATA_SIZE,
/* wMaxPacketSize: */
0x00,
0x00,
/* bInterval */
/*Endpoint 2 Descriptor*/
0x07,
/* bLength: Endpoint Descriptor size */
USB_ENDPOINT_DESCRIPTOR_TYPE,
/* bDescriptorType: Endpoint */
0x02,
/* bEndpointAddress: (OUT2) */
0x02,
/* bmAttributes: Bulk */
VIRTUAL_COM_PORT_DATA_SIZE,
/* wMaxPacketSize: */
0x00,
0x00,
/* bInterval: ignore for Bulk transfer */
/*Endpoint32 Descriptor*/
0x07,
/* bLength: Endpoint Descriptor size */
USB_ENDPOINT_DESCRIPTOR_TYPE,
/* bDescriptorType: Endpoint */
0x03,
/* bEndpointAddress: (OUT3) */
0x02,
/* bmAttributes: Bulk */
VIRTUAL_COM_PORT_DATA_SIZE,
/* wMaxPacketSize: */
0x00,
0x00
/* bInterval: ignore for Bulk transfer */
};
usb_config.h
#define EP_NUM (4) //+EP0
/*-------------------------------------------------------------*/
/* -------------- Buffer Description Table -----------------*/
/*-------------------------------------------------------------*/
/* buffer table base address */
/* buffer table base address */
#define BTABLE_ADDRESS (0x00)
/* EP0 */
/* rx/tx buffer base address */
#define ENDP0_RXADDR (0x40)
#define ENDP0_TXADDR (0x80)
/* EP1 */
/* tx buffer base address */
#define ENDP1_TXADDR (0xC0)
#define ENDP2_RXADDR (0x100)
usb_prop.c
void
Virtual_Com_Port_Reset(
void
)
{
/* Set Virtual_Com_Port DEVICE as not configured */
pInformation->Current_Configuration = 0;
/* Current Feature initialization */
pInformation->Current_Feature = Virtual_Com_Port_ConfigDescriptor[7];
/* Set Virtual_Com_Port DEVICE with the default Interface*/
pInformation->Current_Interface = 0;
SetBTABLE(BTABLE_ADDRESS);
/* Initialize Endpoint 0 */
SetEPType(ENDP0, EP_CONTROL);
SetEPTxStatus(ENDP0, EP_TX_STALL);
SetEPRxAddr(ENDP0, ENDP0_RXADDR);
SetEPTxAddr(ENDP0, ENDP0_TXADDR);
Clear_Status_Out(ENDP0);
SetEPRxCount(ENDP0, Device_Property.MaxPacketSize);
SetEPRxValid(ENDP0);
/* Initialize Endpoint 1 */
SetEPType(ENDP1, EP_BULK);
SetEPTxAddr(ENDP1, ENDP1_TXADDR);
SetEPTxStatus(ENDP1, EP_TX_NAK);
SetEPRxStatus(ENDP1, EP_RX_DIS);
/* pre-fill a packet. */
USB_SIL_Write(ENDP1,(uint8_t *)
''TEST''
, 4);
SetEPTxValid(ENDP1);
/* Initialize Endpoint 2 */
SetEPType(ENDP2, EP_BULK);
SetEPRxAddr(ENDP2, ENDP2_RXADDR);
SetEPTxStatus(ENDP2, EP_TX_DIS);
SetEPRxStatus(ENDP2, EP_RX_VALID);
SetEPRxCount(ENDP2, VIRTUAL_COM_PORT_DATA_SIZE);
/* Set this device to response on default address */
SetDeviceAddress(0);
bDeviceState = ATTACHED;
}
usb_endp.c
/*******************************************************************************
* Function Name : EP1_IN_Callback
* Description :
* Input : None.
* Output : None.
* Return : None.
*******************************************************************************/
void
EP1_IN_Callback (
void
)
{
SetEPTxValid(ENDP1);
}
/*******************************************************************************
* Function Name : EP2_OUT_Callback
* Description :
* Input : None.
* Output : None.
* Return : None.
*******************************************************************************/
void
EP2_OUT_Callback(
void
)
{
packet_receive = 1;
Receive_length = GetEPRxCount(ENDP2);
PMAToUserBufferCopy((unsigned
char
*)Receive_Buffer, ENDP2_RXADDR, Receive_length);
SetEPRxValid(ENDP2);
}
and the 2 endpoint config I just modify usb_desc.c and usb_conf.h
usb_desc.c
const
uint8_t Virtual_Com_Port_ConfigDescriptor[] =
{
/*Configuation Descriptor*/
0x09,
/* bLength: Configuation Descriptor size */
USB_CONFIGURATION_DESCRIPTOR_TYPE,
/* bDescriptorType: Configuration */
VIRTUAL_COM_PORT_SIZ_CONFIG_DESC,
/* wTotalLength:no of returned bytes */
0x00,
0x01,
/* bNumInterfaces: 1 interface */
0x01,
/* bConfigurationValue: Configuration value */
0x00,
/* iConfiguration: Index of string descriptor describing the configuration */
0x80,
/* bmAttributes: Bus powered */
500/2,
/* MaxPower 0 mA */
/*Data class interface descriptor*/
0x09,
/* bLength: Endpoint Descriptor size */
USB_INTERFACE_DESCRIPTOR_TYPE,
/* bDescriptorType: */
0x00,
/* bInterfaceNumber: Number of Interface */
0x00,
/* bAlternateSetting: Alternate setting */
0x02,
/* bNumEndpoints: 3 endpoints used */
0xff,
/* bInterfaceClass: ??? */
0x00,
/* bInterfaceSubClass: */
0x00,
/* bInterfaceProtocol: */
0x00,
/* iInterface: */
/*Endpoint 1 Descriptor*/
0x07,
/* bLength: Endpoint Descriptor size */
USB_ENDPOINT_DESCRIPTOR_TYPE,
/* bDescriptorType: Endpoint */
0x81,
/* bEndpointAddress: (IN1) */
0x02,
/* bmAttributes: Bulk */
VIRTUAL_COM_PORT_DATA_SIZE,
/* wMaxPacketSize: */
0x00,
0x00,
/* bInterval */
/*Endpoint 2 Descriptor*/
0x07,
/* bLength: Endpoint Descriptor size */
USB_ENDPOINT_DESCRIPTOR_TYPE,
/* bDescriptorType: Endpoint */
0x02,
/* bEndpointAddress: (OUT2) */
0x02,
/* bmAttributes: Bulk */
VIRTUAL_COM_PORT_DATA_SIZE,
/* wMaxPacketSize: */
0x00,
0x00
/* bInterval: ignore for Bulk transfer */
};
usb_conf.h
#define EP_NUM (3) //+EP0
Does anybody know how to solve the problem so I can just use 2 endpoint or anybody knows why this error happend?
Thanks in advance
2014-10-01 7:29 AM
''But I
learned
alot from my ''stupid'' trials so I think thats good'' Well, if it works for you - OK then. Bear in mind, most people who learn in an unstructured way and learn it is a hap hazard way - end up coding in the same way. They then wonder why it is really difficult to debug and get something going. ST have provided examples of 4/5 USB device types. This is a good place to start : just understand what a USB device is and how to add/modify enough code to get it to work or do something different. Once, you have tried 2 devices, you will start to understand what I mean by the 'layers' and how ST have partitioned the code into layers to make it easier to understand and work with