cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 PC13 variable duty cycle waveform

RSonn.706
Associate II

I'm intending to use PC13 as an output to drive the onboard LED, but at some point in my program the PC13 pin begins outputting a 4.4 khz signal with pulse width that varies from 0% to 100% back to 0% and keeps repeating that pattern at approx 4 Hz. Is this caused by the RTC calibration function? How can I turn it off. I didn't intentionally turn it on.

1 REPLY 1

Isn't PC13 in the low-power domain? And have very low drive current

Don't enable LSE

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..