cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F101x4 IAR version

jgalea
Associate II
Posted on February 02, 2009 at 03:37

STM32F101x4 IAR version

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
jgalea
Associate II
Posted on May 17, 2011 at 13:01

Hello, Can anyone notify me if the IAR EWARM-KS-WEB-5301.EXE is suitable for the low density micro STM32F101x4? I was using the IAR version that comes with development board STM32-SK, and the program was halting during download. Im suspecting that this IAR version is not suitable for STM32 low density micros. Thanks Johann

jilisegiar
Associate II
Posted on May 17, 2011 at 13:01

Yes the new version 5.30 is suitable with the low denstity devices:

http://www.iar.com/website1/1.0.1.0/94/1/index.php?

jgalea
Associate II
Posted on May 17, 2011 at 13:01

This is is the same one I downloaded. Can anyone help me how to set it to work on STM32F101C4. I'm sending the error message I'm obtaining in a doc file. Thanks Johann

jilisegiar
Associate II
Posted on May 17, 2011 at 13:01

just select ''ST STM32F10xx4'' as device name in options->target->Device

and check that the flash loader is set to default.

jgalea
Associate II
Posted on May 17, 2011 at 13:01

Hello jilisegiar. Thanks for your reply. Can you please indicate to me the file that I need to download? Many thanks Johann I downloaded 5.4 and is not working on the low end micro. Thanks Johann

jgalea
Associate II
Posted on May 17, 2011 at 13:01

Hello jilisegiar, Thanks very much it worked. Johann