2010-07-09 12:09 AM
STM32F100 value line TIM15/16/17 SFR
2011-05-17 4:58 AM
I have a board (our custom hardware) with a STM32F100C6T6B on it. Its running (my) firmware that has exception detection and handling in it.
I just added the following code to see if I could reproduce your issue. temp = TIM15 -> CR1; temp = TIM16 -> CR1; temp = TIM17 -> CR1; The above ran without issue (no fault generated). Are you sure you have a Value Line (F100) device? Timers 15-17 don't exist in other families.2011-05-17 4:58 AM
Thank you for testing that.
I am sure that it is a STM32F100 derivate and not F101 or F103. Could it be, that this controller has a defect memory region? Maybe i will solder another one on the board. First I will have a look for possible software issues.2011-05-17 4:58 AM
Do you have alpha or beta version silicon (I know we had beta stuff)? The STM32F100 is quite new so its possible you have buggy chips.
2011-05-17 4:58 AM
I changed the processor and now it works. Seems that some of the processors memory was defectous. This looks very strange to me. I never have seen something like this before. How is it possible that some (only a few) memory regions can be defectous?
I don't know if i have beta-chips. I have 5 and 5 samples and assume that they are from different production lots. The last 5 from package marking are: MYS 018 and MYS 940.2011-05-17 4:58 AM
The STM32F100C6T6B I'm using is marked
9903N VC MYS 009 Z I don't see anything listed in the (which is for rev Z which is what I have) but there is timer (1-5) issues listed in there.2011-05-17 4:58 AM
I checked two further controllers with MYS 940 production lot. They also showed the problem when accessnig the MCU-registers of Timer 15 to 17.
Seems that i have received defectous chips.