2020-02-27 09:57 AM
2020-02-29 04:18 AM
BTW, the time quanta settings look different from the standard, because the standard says thet the SYNC_SEG is always 1. It doesn't need to be configured. Alsi in STM32 bxCAN, the TimeSeg1 contains the sum of both PROP_SEG and PHASE_SEG1.
And no, there is no "Motorola CAN", "Intel CAN" or "STMicro CAN". Just CAN.