2017-02-26 3:32 AM
Hi everybody,
I am facing a rather strange problem when trying to program the two user option bytes (0x1ffff804, 0x1ffff806).
The code I am using is rather straightforward:
volatile
FLASH_Status
test3;
volatile
uint8_t
test, test2;test = 0x12;
test2=0;
FLASH_Unlock();
FLASH_OB_Unlock();
test3 = FLASH_OB_ProgramData( 0x1FFFF804, test);
FLASH_OB_Launch();
FLASH_OB_Lock();
FLASH_Lock();
test2 = FLASH_OB_GetUser();
The code il flashed on a Nucleo64 board. Apparently the CPU hangs completely when executing FLASH_OB_Launch().
If I step the code through the instructions, it looks as if FLASH_OB_Launch() is generating a complete erase of the chip. In fact, I cannot simply reset and re-start execution, I need to re-load the program with the debugger.
If I remove FLASH_OB_Launch() the code executes with no problems, test3 reports FLASH_COMPLETE but the options bytes are not programmed.
I can read and program the option bytes without any problem using ST-link.
Elsewhere in the code I am erasing and programming the flash memory again with no problems, but the options bytes just do not program!
Can anybody please give me a hint?
Regards,
Gabriele
2017-03-12 7:56 AM
Hello Gabriele
I've had more or less the same problem: CPU crashes (I lose connection with the debugger) when I execute FLASH_OB_Launch(). But I figured out that it is not needed to program the two free bytes at 0x1FFFF804 and 0x1FFFF806.
Whatsoever, I had to first call FLASH_OB_Erase() before FLASH_OB_ProgramData() to get it work.
Hope it helps,
regards
2017-03-12 4:19 PM
Hi Renato,
apparently -I read it in the documentation- FLASH_OB_Launch() forces a reset of the CPU to get the data programmed. This could be the reason why the debugger loses the connection and the CPU hangs.
Anyhow, as I could also not live with a CPU reset in that situation, I simply overcame the problem by just using a page of the flash memory, which I now use as a “quasi-ram�.
The positive side-effect is that I can now make use of many more “flash� bytes than just two!
Best regards,
Gabriele