STM32F072CB EXTI
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-04-29 9:35 AM
Posted on April 29, 2015 at 18:35
Hi all,
I have a problem again. We using STM32F072CB LQFP48 controller in a project where we connected an encoder to PC14 and PC We don't use external clock source. So I enabled GPIO clock for GPIOC, set PC14 and PC15 as input with Pull-Up, set EXTI4->EXIT14 and EXTI15 to GPIOC and enable interrupt. My problem is the EXTI4_15 interrupt handler receives interrupt continuously and I don't understand why. Here is the code snipet:#define ENC_A GPIO_Pin_15
#define ENC_B GPIO_Pin_14
#define PENC_A GPIOC
#define pENC_A GPIOC, ENC_A
#define pENC_B GPIOC, ENC_B
#define EC10E_ENCODER_IRQ_DISABLE()\
{\
NVIC_DisableIRQ(EXTI4_15_IRQn);\
}
void Ec10e_encoder_Init(void)
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
//1. Configure the GPIO as input
//Init_GPIO_Mode(pENC_A | ENC_B, GPIO_Mode_IN);
GPIO_InitTypeDef InitGpio;
InitGpio.GPIO_Pin = ENC_A | ENC_B;
InitGpio.GPIO_Mode = GPIO_Mode_IN;
InitGpio.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(PENC_A, &InitGpio);
//2. Ensure pull up resistor is enabled, pull down resistor is disabled
// is connected to Pushbutton
PENC_A->PUPDR &= ~(GPIO_PUPDR_PUPDR14 | GPIO_PUPDR_PUPDR15);
PENC_A->PUPDR |= (GPIO_PUPDR_PUPDR14_0 | GPIO_PUPDR_PUPDR15_0);
//3. Clear bits 11:8 and 15:12 and set 0 in the SYSCFG_EXTICR[4] reg to amp EXTI Line to NVIC
//ENC_A:
SYSCFG->EXTICR[4] &= (uint16_t)~(SYSCFG_EXTICR4_EXTI14 | SYSCFG_EXTICR4_EXTI15);
SYSCFG->EXTICR[4] |= (uint16_t) (SYSCFG_EXTICR4_EXTI14_PC | SYSCFG_EXTICR4_EXTI15_PC);
//4. Set interrupt trigger to falling edge on the EXTI1 line
EXTI->FTSR |= (EXTI_FTSR_TR14 | EXTI_FTSR_TR15);
EXTI->RTSR &= ~(EXTI_RTSR_TR14 | EXTI_RTSR_TR15);
//5. Unmask EXTI0 line
EXTI->IMR |= (EXTI_IMR_MR14 | EXTI_IMR_MR15);
EXTI->EMR &= ~(EXTI_IMR_MR14 | EXTI_IMR_MR15);
//6. Set Priority to 3
NVIC_SetPriority(EXTI4_15_IRQn, 3);
//7. Enable EXTI4_15 interrupt in NVIC (do 4 first)
EC10E_ENCODER_IRQ_ENABLE();
}
/// @brief EXTI_4_15_IRQHandler for encoder (ENC_A, ENC_B; GPIO_Pin_15, GPIO_Pin_14; PC15, PC14).
/// @param None
/// @retval None
void EXTI4_15_IRQHandler(void)
{
if ((EXTI->IMR & EXTI_IMR_MR14) && (EXTI->PR & EXTI_PR_PR14))
{
//I always receive this interrupt even if the encoder is in stable state.
EC10E_ENCODER_IRQ_DISABLE();
EXTI->PR |= EXTI_PR_PR14;
}else
if ((EXTI->IMR & EXTI_IMR_MR15) && (EXTI->PR & EXTI_PR_PR15))
{
EC10E_ENCODER_IRQ_DISABLE();
EXTI->PR |= EXTI_PR_PR15;
}
}
//-----------
Thank you!
#stm32f072cb #exti
Labels:
- Labels:
-
GPIO-EXTI
-
STM32F0 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-04-29 4:06 PM
Posted on April 30, 2015 at 01:06
I forgot to mention that the IDE is Coocox CoIDE.