cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030C8 - does support for the Unique Device ID ?

PRAJ.205
Associate

We have developed the product with the STM32F030C8 , now we are going for the Mass production .

But different device ID for the different product , can we use the Unique device ID for the same .

1 ACCEPTED SOLUTION

Accepted Solutions

The 'F030 does not support the factory-provided Unique device ID. You'd need to use STM32F051C8, which is an identical chip to the 'F030, except that it has some of the features such as wider temperature range and also the unique device ID, at an increased price.

You can also put your own serial number into the FLASH when programming the devices.

JW

 https://community.st.com/s/question/0D50X00009XkfKFSAZ/stm32f0-unique-id-location

View solution in original post

1 REPLY 1

The 'F030 does not support the factory-provided Unique device ID. You'd need to use STM32F051C8, which is an identical chip to the 'F030, except that it has some of the features such as wider temperature range and also the unique device ID, at an increased price.

You can also put your own serial number into the FLASH when programming the devices.

JW

 https://community.st.com/s/question/0D50X00009XkfKFSAZ/stm32f0-unique-id-location