2018-04-02 2:26 AM
Hi, I have a STM32F0C6 board and I'm trying to use RTC function with LSE.
It seems RTC is working correctly and I can check the waveform of LSE Clock from MCO pin.But when I check the waveform of OSC32_IN and OSC32_Out pins by using an OscilloScope,OSC32_IN: about 300mV flat lineOSC32_Out: about 1.3V waveform nearly LSE clock(32.768KHz).Is this correct work of OSC32_IN and OSC32_Out?
please give me an information.
and let me apologize for my poor English.thank you.2018-04-02 6:24 AM
The LSE oscillator is a very low power (thus high impedance) analog circuit, thus it is very easy to be influenced by the attached oscilloscope probe (which presents a significant load).
JW
2018-04-02 6:37 AM
sounds about right. probing the output pin is better, as its impedance is lower.
2018-04-02 7:27 AM
you can use a 1Meg resistor in series with your probe,
then the oscillator should keep working whilst you are watching it.
but you will shift the frequency with the probe capacitance.
henry.****
is correct, you should be probing the output pin.