2017-07-26 05:19 AM
Hi All,
A brief background:
I'm a
hardware
guy and new to all things ARM and STM32 MCUs. I've now jumped on board because ST has an agreement with Keil for STs Cortex M0/M0+ MCUs. I've programmed before but only 8-bit MCUs in Arduino and the CCS PIC C compiler from Custom Computer Services for the Microchip PIC line of MCUs.For my very first project, I’ve begun work on phase angle control of the T1235 TRIAC also from ST. The processor I’m using is a Cortex M0 from the STM32F0 series. I’ve used STM32CubeMX (again for the first time ever) to generate the initialization code and have written some code in Keil uVision 5 (using this for the first time too). I’m using an opto-TRIAC in between the MCU and the T1235. I also have a zero-crossing detector (ZCD) that gives a pulse to the MCU every 10ms (50Hz mains).
So far, I’ve been able to trigger the TRIAC into a fully ON state and implement some crude dimming. Crude because the dimming does not work properly as the incandescent lamp flickers annoyingly even though.
The code implemented is something along the lines of this:
http://www.electronicsinfoline.com/pin/38328/2/
The ZCD signal is fed to the external (EXTI) interrupt. Now, to stabilize this and get smooth control with no flicker, I need to use one or perhaps more timers.
So far, I’ve referred to the MCU datasheet, errata sheet for device limitations and the following resources:
UM1785 – HAL user manual
RM0360 – Reference manual
AN4776 – General purpose timer cookbook
PM0215 – Cortex M0 programming manual
Technical ref manual for the ARM-CortexM0
AN4013 - STM32 cross-series timer overview
A whole bunch of YouTube videos
A search for ready-made drivers
Now, I will admit that I’ve not read all the above pdfs in great detail but I simply have not been able to find or understand (whatever I have found) how the timer hardware within my processor functions. Furthermore, STs documentation leaves a lot to be desired.
I was thinking of implementing the following logic which needs a good understanding of how timers function. An interrupt starts the timer that’s being clocked and it gives a small (100usec) pulse to fire the TRIAC at very regular intervals.
My questions are:
Can someone please explain (or point me in the right direction) in detail how the STM32F0 timers work since I apparently can’t seem to follow what’s written in RM0360 and AN4776.
Are there any other resources / videos that will explain how to better use the HAL.
Thanks in advance
2017-07-26 06:59 AM
Hello
sid
,can you please tell us, what exactly is not clear on how timers work? What functionality on timer you would like to use? PWM, Input capture, output compare, etc.
Best regards,
Tilen
2017-07-26 09:02 AM
Hello!
Nice work!
The triac gate must be pulsed as soon as posible the Mains passing zero voltage(and power) to switch on. (be aware from capacitive and inductive loads)
The Timer configuration you need is One Pulse Mode triggered by the zero-crossing detection circuit.
and connected to a GPIO pin as PWM output
you must have at least 1 as TIMx ARR (zero value will block the timer)
and 1 (least) at PWM Pulse (1 microsecond) This is the delay from trigger to start the pulse(phase) ~1 micro (can not be zero.. Blocks the Output)
your ''pulse width'' is TIMx ->ARR - PWM Pulse
The max duty cucle at your pulse is ~10000 <10 millisecond
Depending your configuration you can change the polarity of triger(connected to ZCD)
Just to know I dont have the hardware you own.
I tried this configuration at 32L152 and 32F4 three boards.
2017-07-26 11:24 AM
Ha ha that's just it, even i'm not so sure! Apologies for not asking narrower/exact questions!
Thank you for the prompt reply Tilen Majerle!
Since I'm used to the 8-bit PICs, my first thought was something like this:
1) Configure Interrupt
2) Interrupt (from ZCD) starts timer counting. Timer counts (either increments or decrements) from internal clock. It does not count the ZCD pulses.
3) Specifically for my application of firing a TRIAC on 50Hz AC mains, timer minimum value = 500usec / max value = 9500usec
4) Once set time (a value anywhere between the above mentioned limits) lapses, a 100usec or 200usec pulse fires the TRIAC. This is to take place periodically.
While the timers are 'chopping the AC mains' the time period needs to be stable and unchanging to avoid flicker.
Other than my above mentioned 4 step method, I'm open to other approaches btw!
Now, PWM doesn't help, neither does input capture. I'm unsure if output compare would help here? I'm unclear how that works.
As far as '
what exactly is not clear on how timers work
' - In the PIC uCs the documentation is easy to understand. But with ST, the documentation is not only unclear and very generic but the timers and their functionality is just too vast. Furthermore most acronyms ST uses are not very self explanatory (apologies again, don't mean to offend anyone). Even after reading the pages that explain all registers associated with the Timers, this too didn't help me make up my mind as how I'm supposed to configure the MCU to output a super stable one shot at regular intervals after an interrupt occurs on EXTI.I can't seem to figure out how to appropriately configure the timers, their pre-scalers, the auto reload registers or capture compare registers, especially to achieve what i said in point 4 above. I hope I've been specific enough. Thanks.
2017-07-26 03:27 PM
What is your MCU exactly? to give you a better proposition!!
Post also other hardware details. . Does the ZCD gives positive pulse when pass from zero?
What polarity must be the pulse have to triger the optocoupled DIAC (consider to use an open colector output from MCU)
2017-07-27 12:19 AM
MCU is STM32F030F4
ZCD gives a falling edge output
A high pulse drives the opto-TRIAC that in-turn drives the main TRIAC
2017-07-27 04:40 AM
2017-07-27 05:18 AM
Thank you Vangelis for taking the trouble to help me and illustrate this with print screens. It's much appreciated!
I'll let you know how it turned out.
2017-07-27 06:24 PM
Hi,Here is what you need for this:
set the following option in the Timer register (they vary with the Timer and channel used so refer to the reference manual):
have fun
Yves
2017-08-17 01:04 AM
Hello Vangelis,
Sorry for the delay. I got pulled away from this due to unavoidable circumstances.
Anyway I tried out the code you so kindly typed out. It didn't work. Instead something strange happened. The ZCD input went high even though i configured everything exactly as you've mentioned. The TRIAC never fires no matter what the value of
SetPhasePercent(value); is set to
. A print screen of my configuration in STM32CubeMX is attached here in. The code's a copy-paste of yours as above. All other settings remain unchanged.Thank you for your help.