STM32F0-disco printf USART
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-22 9:50 PM
Posted on May 23, 2018 at 06:50
Hi, I'm working with the STM32F0 Discovery board.
I have a problem to use printf function with the USART.I'm using the classical way to redirect printf function (redefine _io_putchar and added _write function).
So printf works great when I use the IDE to compile and flash (I use SW4ST32).But when i try to compile and flash in command line using the same commands as the IDE, the printf function does nothing. The _write function works but is not called by printf.
To compile in command line i get all the .o files generated by the IDE and i compile the main file and then link everything together.So my question is, What could be the reason for printf to not call the _write function ?
Thanks
0 REPLIES 0