cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Discovery RTC issue with CubeMX

maciej1
Associate
Posted on January 26, 2015 at 19:30

Hello, I've tried to run default RTC configuration at STM32L Discovery demo board using cubeMX but even if I tried to switch between clocks my code always get error with function:

RTC_EnterInitMode() in ''Wait till RTC is in INIT state and if Time out is reached exit''

-So my RTC is never in init state. 

Yes I change WPR bits to 0xCA, 0x53 (CubeMx make it for me using __HAL_RTC_WRITEPROTECTION_DISABLE() macro)

Due this I always got 0 from TR RTC register, also alarms don't works for me.

I tried with switching RTC sources (HSE, LSE, LSI) but always the same effect and empty struct

Also set PWR_CR bit before clock configuration didn't help.

Can You check if stm32L152 works with cubeMX software? Or give me some tips how to run it.

#discovery #stm32l152 #cubemx
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0