2018-04-28 11:10 AM
I downloaded the STM32CubeProg from the STM website. It appears to install a couple of USB drivers. However, it does not recognize my custom STM32F7 board that is in DFU mode. Per the User Guide I have uninstalled the DfuSe USB driver, but the
STM32CubeProg still cannot see my board. If I reboot my board, the DfusSe drivers are automatically re-installed by Windows. Am I doing something wrong?
2018-05-02 05:36 AM
Hello
Hooper.Mike
,Do you get an error message ?
Please, confirm if you have the same issue in this
https://community.st.com/0D70X000006SskYSAS
, as there is a known issuewithSTM32CubeProgrammer to connect with STM32F7 board and will be fixed in the coming release.https://community.st.com/0D70X000006SskYSAS
Best Regards,
Imen
2018-05-02 08:04 AM
No error message. The STM32CubeProg simply does not recognize the USB DFU device.
2018-05-02 08:34 AM
Hi Mike,
You may try the proposition to use zadig program or
force the update to the new driver
as mentioned in this discussionhttps://community.st.com/0D50X00009XkXagSAF
.Please keep me informed about your progress on this.
Best Regards,
Imen
2018-05-21 02:42 AM
Hello Mike,
Can you please precise which device ID are you using ?
Best Regards,
Imen.
2018-05-22 06:29 AM
Imen,
I am using the STM32F765VIT6.
Thanks,
Mike