2016-09-16 3:56 PM
Hi,
I used to work on STM32F4 and now are evaluating STM32F7. When I tried to create a project with STM32F769NI with SPI. I found that I can't set the Prescaler to 2 (APB2 = 108Mhz) which will result the SPI6 to 54Mhz.The error message is ''With this Prescaler value and APB2 Clock Frequency (108.0 MHz), Baud Rate is more than : 50.0 MBit/s. But the datasheet clear said it can go up to 54MHz. So..The program is wrong, datasheet is wrong or I am wrong? (SPI 6, master mode with full duplex). I also set the voltage to 3.3. Regards,TYY #stm32f7-spiSolved! Go to Solution.
2017-01-02 7:15 AM
Original issue has been fixed in 4.18 release: 'With SPI on STM32F769NI, set the Prescaler to 2 (APB2 = 108Mhz), set the voltage range to 3.3 V. With this Prescaler value and APB2 Clock Frequency (108.0 MHz), maximum Baud Rate is 50.0 MBit/s when we should be able to reach SPI6 at 54Mhz'.
Indeed:
- The max value depends on voltage range. So 54MHz, should be proposed if application is running 3.3V typical. - At low voltage range, the delay on the pad is longer and limits the max frequency.2016-09-19 6:49 AM
Hi,
Could you precise which version of CubeMx are you using ?Regards2016-09-19 6:52 AM
Hi TONYY,
Could you please precise which CubeMX version are you using?If you are using an old version, I recommend you to use the latest: 4.16.1-Syrine-2016-09-19 8:17 AM
I believe I am at 4.1, I updated it a few days ago.
Tony ________________ Attachments : mx1.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htpy&d=%2Fa%2F0X0000000aXY%2FiGZs30_ue3xJUrRsLR3eCwkyvW8opMaKfxX5cwy2ljk&asPdf=falsemx2.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtmW&d=%2Fa%2F0X0000000aWq%2FwcU8mog91BamfjasxxtdL03tdn19U1rgbetxY9rbSa8&asPdf=false2016-09-20 1:45 AM
Hi TONYY,
Thank you for your feedback. The issue has been reported internally.-Syrine-2017-01-02 7:15 AM
Original issue has been fixed in 4.18 release: 'With SPI on STM32F769NI, set the Prescaler to 2 (APB2 = 108Mhz), set the voltage range to 3.3 V. With this Prescaler value and APB2 Clock Frequency (108.0 MHz), maximum Baud Rate is 50.0 MBit/s when we should be able to reach SPI6 at 54Mhz'.
Indeed:
- The max value depends on voltage range. So 54MHz, should be proposed if application is running 3.3V typical. - At low voltage range, the delay on the pad is longer and limits the max frequency.