2018-08-21 3:20 AM
Hello,
Since the last update of STM32CubeMX 4.26.1, I can't open my project file anymore.
Right after clicking on the 'open' button, the software freezes and one of the processor cores stays at 100%. The only available action, then, is to close the application.
As I can't download an older version of STM32CubeMX, I am out of options.
I attached the project file in question to this post.
Thanks in advance for your help.
2019-07-13 12:19 AM
I have CubeMx version 5.2.1 and I cannot open an IOC project made with TouchGFX.
The error I get is :
2019-07-13 08:53:41,769 [INFO] ApiDbMcu:444 - Load IP Config File for GRAPHICS
Exception in thread "AWT-EventQueue-0" java.lang.ArrayIndexOutOfBoundsException: 8
at com.st.microxplorer.plugins.projectmanager.gui.ProjectChoiceTab.updateToolChainSelection(ProjectChoiceTab.java:1895)