2017-02-13 2:52 AM
I am using STM32CubeMX Version 4.16.1 on a pc without(!!!) internet access.
I would like to install a new library via 'Menu'/'Help'/'Install New Libraries'/'From Local...'.I have downloaded the firmware package for family STM32F4 (Software Version 1.14.0) ===> 'en.stm32cubef4.zip'When i try to install this firmware package by pressing the 'From Local...'-button and by selecting the downloaded zip-file 'en.stm32cubef4.zip',i receive the following error message 'This package version is not managed on this version of STM32CubeMX'.Anything i can do about this?I tried to download the firmware package for family STM32F4 in an earlier version (for example 1.13.0) but i could notfind it on the internet.Any help would be greatly appreciatedSolved! Go to Solution.
2017-02-13 3:07 AM
Hi
mondaymorning
,TheSTM32F4 version 1.0 is not supported by the MX4.1 ,it is supported since the MX version 4.18 and also on the last MX version 4.
So, I recommend you to install the last MX 4.
-Nesrine-
2017-02-13 3:07 AM
Hi
mondaymorning
,TheSTM32F4 version 1.0 is not supported by the MX4.1 ,it is supported since the MX version 4.18 and also on the last MX version 4.
So, I recommend you to install the last MX 4.
-Nesrine-
2017-02-13 4:55 AM
Hi Nesrine!
Thank you for that hint
Just downloaded the MX4.16.1 a few days ago. Didn't know there is already an updated version.
Ok, now i have installed MX 4.19 and the installation of the firmware package for family STM32F4 (Software Version 1.14.0 / en.stm32cubef4.zip) runs smoothly.
Best regards
Tobias
2017-09-05 3:41 AM
Thanks Clive,
As I am pretty new in the STM environement and as I understand we can not use this HAL directely in the Cube MX? If no, in cube mx, can we instead use the STM32L0 library, in fact the STM32L072CZY6TR? I will use the discovery as a NUCLEO without using the Lora Semtech chip...
2017-09-05 4:06 AM
Hello,
Today I run into the same problem. I download the latest Cube MX 4.22.00, install new library 'en.i-cube_lrwan.zip' and I got the same message 'This package version is not managed on this version of STM32CubeMX'.
Anyone can help?Regards
Alex
2017-09-05 5:20 AM
It is a stand alone HAL package, not some plug in to CubeMX. Just unzip into its own directory.
2017-09-05 8:36 AM
CubeMX is a code generator, the code is output using the HAL library as a foundation. The LRWAN stuff was written by a group of people using the HAL library, rather than using an automated tools. ST slaps 'Cube' on things as branding, a bit like Microsoft calling a whole range of dissimilar things .NET
You can build L0 based projects using CubeMX, merging that back into the LRWAN code base might prove quite challenging, but if you just want to blink LEDs and get comfortable with the NUCLEO board that should be fine.