cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX ''modified'' status of *.ioc files

qwer.asdf
Senior
Posted on October 20, 2015 at 10:24

Hi, it's a small but annoying bug, every time I open my *.ioc project file (which was gradually migrated 5-6 times from older versions) Cube immediately marks the project as modified (asterisk in the title just after the file name) and annoyingly asks to save the file when closing the Cube even when I changed nothing. Even when I agree to save the ''changes'', the next time I open the project it's in ''modified'' state again.

14 REPLIES 14
Posted on May 11, 2017 at 21:17

I have to correct myself. Currently I'm using 4.19

Posted on May 12, 2017 at 00:59

Ubuntu 16.0.4.1

openjdk version '1.8.0_121'

CubeMX 4.20.1

for STM32F777NIHx and STM32F765NIHx

Windows 7

Java 1.8.0_131

CubeMX 4.21

for STM32F777NIHx and STM32F765NIHx

Posted on May 12, 2017 at 09:36

Hello David,

Thank you for your sharing.

I success to reproduce it by openning RCC or CORTEXM7 configuration panel only.

If I select NVIC or DMA, and press cancel, star does not appears.

We are investiguating this issue from that angle.

Kind regards

Sirma

Posted on May 12, 2017 at 09:38

Hello Br_ggemann.Dieter,

We finaly sucess to reproduce it, by selecting RCC or CORTEX M7 configuration panel on F777 SoC.

Kind regards

Sirma

Sirma Siang
ST Employee
Posted on June 30, 2017 at 12:20

Hello All,

I am pleased to inform you that this anoying issue will be fixed in verion 4.23.

This release will be available in October.

Kind regards

Sirma