2015-10-20 01:24 AM
Hi, it's a small but annoying bug, every time I open my *.ioc project file (which was gradually migrated 5-6 times from older versions) Cube immediately marks the project as modified (asterisk in the title just after the file name) and annoyingly asks to save the file when closing the Cube even when I changed nothing. Even when I agree to save the ''changes'', the next time I open the project it's in ''modified'' state again.
2017-05-11 02:17 PM
I have to correct myself. Currently I'm using 4.19
2017-05-11 05:59 PM
Ubuntu 16.0.4.1
openjdk version '1.8.0_121'
CubeMX 4.20.1
for STM32F777NIHx and STM32F765NIHx
Windows 7
Java 1.8.0_131
CubeMX 4.21
for STM32F777NIHx and STM32F765NIHx
2017-05-12 02:36 AM
Hello David,
Thank you for your sharing.
I success to reproduce it by openning RCC or CORTEXM7 configuration panel only.
If I select NVIC or DMA, and press cancel, star does not appears.
We are investiguating this issue from that angle.
Kind regards
Sirma
2017-05-12 02:38 AM
Hello Br_ggemann.Dieter,
We finaly sucess to reproduce it, by selecting RCC or CORTEX M7 configuration panel on F777 SoC.
Kind regards
Sirma
2017-06-30 03:20 AM
Hello All,
I am pleased to inform you that this anoying issue will be fixed in verion 4.23.
This release will be available in October.
Kind regards
Sirma