2015-11-17 5:51 PM
I have a project that is using USART1 on an STM32F301R8.
The initialization code that CubeMX generates for USART1 includes a reference to ''RCC_USART1CLKSOURCE_PCLK1'', which does not exist in stm32f3xx_hal_rcc.h . There are equivalent symbols for USART2 and USART3, but there seems to be a missing block for USART1. STM32CubeMX version: 4.10.1 (I'm currently updating to 4.11.0, but figured I'd write this up while I wait to see if that fixes it.) Firmware Package for Family STM32F3 version: 1.2.0 I can attempt to make a minimal example for this, but given that the USART1 block seems to be missing from stm32f3xx_hal_rcc.h, I don't think this one will be hard to track down.2015-11-18 5:38 AM
Hi Izzy84075,
I will check this problem with our development team & come back to you.Sorry for the inconvenience it may bring.-Syrine-2015-11-18 11:28 AM
Updating to CubeMX Version 4.11.0 and STM32F3 Firmware Package Version 1.3.0 does not fix this.
2015-11-19 1:51 AM
Hi Izzy84075,
The reported issue is under review, it is not a CubeMX issue, it seems to be related to a miss define of the STM32F301 in the stm32f3xx_hal_rcc_ex.h -Syrine-2015-11-20 9:02 AM
Hi Izzy84075,
Your reported issue is confirmed by our team and will be fixed in coming release of the STM32cubeF3 package.Thank you very much for your contribution to the enhancement of our STM32 related solutions.-Syrine-