cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX version inconsistency

Posted on November 20, 2015 at 02:20

As far as I know, the current version of CubeMX is 4.11.00.

I'd downloaded the windows installer for the standalone version STM32CubeMX from http://www.st.com/web/en/catalog/tools/PF259242 and it works as expected.

Then, for some reason, I also need to install the eclipse plugin and find the STSW-STM32095 at http://www.st.com/web/en/catalog/tools/PF257931, and it was also labeled with version 4.11.0.

But then, after installation and trying out, I find out that the downloaded plugin was no version 4.11.0 but an older 4.10.1 instead.

As a consequence, the plugin refuses my project when trying to open with the message:

The Firmware Package (STMCube FW_F4 V1.9.0) required by the Project is not supported by this Stm32CubeMX version. to use this Project, update your Stm32CubeMX installation to the latest version.

When looking into the zip archive of the download, I find a site.xml which contains:

feature url=''features/com.st.microxplorer_4.10.1.201509281014.jar'' id=''com.st.microxplorer'' version=''4.10.1.201509281014''

And further, when I create a new project with the cubemx plugin, the myproject.ioc contains a:

MxCube.Version=4.10.1

Could ST please provide the eclipse plugin for the most recent version 4.11.0?

Joe

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 02, 2016 at 19:53

Hi Shahrzad,

nice to see, that this issue is solved with CubeMX 4.12.0.

Cheers, Joe.

Posted on November 20, 2015 at 17:45

Hi Joe,

I confirm the problem, It will be fixed as soon as possible. sorry for the inconvenience it may bring.

-Shahrzad-