2018-07-02 3:08 PM
I'm trying to build a simple 'hello world' program on the STM32H743 using the Makefile option and the standard Ubuntu arm-none-eabi-gcc V 4.9.3. At this stage my program doesn't even do floating point, but it will eventually, so I'd like to get the h/w floating point working. The link fails with:
/usr/lib/gcc/arm-none-eabi/4.9.3/../../../arm-none-eabi/bin/ld: failed to merge target specific data of file build/stm32h7xx_hal_i2c.o
/usr/lib/gcc/arm-none-eabi/4.9.3/../../../arm-none-eabi/bin/ld: error: build/stm32h7xx_hal_rcc_ex.o uses VFP register arguments, build/test_H7.elf does notEvery object gets listed with the above error, I've just used stm32h7xx_hal_rcc_ex.o as an example. All objects get compiled with: -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard as per the switches in the Makefile generated by CubeMX (V 4.25.1) The STM32Cube MCU Package for STM32H7 is version 1.2.0.
2018-07-02 3:21 PM
So sounds like the compiler builds the objects properly. Focus the settings the linker is using.
2018-07-02 6:10 PM
Using 4.9.3 under Windows to build for the STM32H743I-EVAL, something based on the HAL UART demo rather than CubeMX stuff.
Assembling file: startup_stm32h743xx.s
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -g -ggdb3 -Wa,-amhls=out/startup_stm32h743xx.lst -DUSE_HAL_DRIVER -DSTM32H743xx -DUSE_STM32H743I_EVAL -MD -MP -MF out/startup_stm32h743xx.d -I. -Iinc startup_stm32h743xx.s -o out/startup_stm32h743xx.oLinking target: out/demo.elf
arm-none-eabi-g++ -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -TSTM32H743XIHx_FLASH.ld -g -Wl,-Map=out/demo.map,--cref,--no-warn-mismatch -Wl,--gc-sections -nostartfiles out/startup_stm32h743xx.o out/main.o out/stm32h743i_eval.o out/stm32h7xx_hal.o out/stm32h7xx_hal_cortex.o out/stm32h7xx_hal_gpio.o out/stm32h7xx_hal_msp.o out/stm32h7xx_hal_rcc.o out/stm32h7xx_hal_rcc_ex.o out/stm32h7xx_hal_uart.o out/stm32h7xx_it.o out/syscalls.o out/system_stm32h7xx.o -o out/demo.elfCreating extended listing: out/demo.lss
arm-none-eabi-objdump -S out/demo.elf > out/demo.lssCreating memory dump: out/demo.dmp
arm-none-eabi-objdump -x --syms out/demo.elf > out/demo.dmpCreating IHEX image: out/demo.hex
arm-none-eabi-objcopy -O ihex out/demo.elf out/demo.hexCreating binary image: out/demo.bin
arm-none-eabi-objcopy -O binary out/demo.elf out/demo.binSize of modules:
arm-none-eabi-size -B -t --common out/startup_stm32h743xx.o out/main.o out/stm32h743i_eval.o out/stm32h7xx_hal.o out/stm32h7xx_hal_cortex.o out/stm32h7xx_hal_gpio.o out/stm32h7xx_hal_msp.o out/stm32h7xx_hal_rcc.o out/stm32h7xx_hal_rcc_ex.o out/stm32h7xx_hal_uart.o out/stm32h7xx_it.o out/syscalls.o out/system_stm32h7xx.o text data bss dec hex filename 786 0 0 786 312 out/startup_stm32h743xx.o 2516 0 128 2644 a54 out/main.o 1676 24 176 1876 754 out/stm32h743i_eval.o 1250 5 4 1259 4eb out/stm32h7xx_hal.o 646 0 0 646 286 out/stm32h7xx_hal_cortex.o 902 0 0 902 386 out/stm32h7xx_hal_gpio.o 212 0 0 212 d4 out/stm32h7xx_hal_msp.o 2734 0 0 2734 aae out/stm32h7xx_hal_rcc.o 5288 0 0 5288 14a8 out/stm32h7xx_hal_rcc_ex.o 5448 0 0 5448 1548 out/stm32h7xx_hal_uart.o 18 0 0 18 12 out/stm32h7xx_it.o 272 4 8 284 11c out/syscalls.o 424 8 0 432 1b0 out/system_stm32h7xx.o 22172 41 316 22529 5801 (TOTALS)Size of target .elf file:
arm-none-eabi-size -B out/demo.elf text data bss dec hex filename 34760 2228 1732 38720 9740 out/demo.elf