2017-02-20 1:57 PM
Everyone,
How can I use cubeMX for SDcard ? I have generated for MDK but :
this function doesn't work , from UM1721
User manualDeveloping Applications on STM32Cube with FatFs page 21.:
uint32_t wbytes; /* File write counts */
uint8_t wtext[] = 'text to write logical disk'; /* File write buffer */if(FATFS_LinkDriver(&mynewdisk_Driver, mynewdiskPath) == 0){if(f_mount(&mynewdiskFatFs, (TCHAR const*)mynewdiskPath, 0) == FR_OK){if(f_open(&MyFile, 'STM32.TXT', FA_CREATE_ALWAYS | FA_WRITE) == FR_OK){if(f_write(&MyFile, wtext, sizeof(wtext), (void *)&wbytes) == FR_OK);{f_close(&MyFile);}}}}FATFS_UnLinkDriver(mynewdiskPath);This variable :
&mynewdisk_Driver doesn't exist, which file is related ?
Thank you
2017-02-25 4:15 AM
I got until this if, but the code is stopped here ,
Is SDCard initialized properly already ?
if(f_open(&MyFile, 'Hello.txt', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK)
2017-02-26 3:09 AM
I'm confused, so sdio and SD card isn't yet initalized ??
2017-02-26 8:14 AM
Hi
No, FATFS can run on different backends not only SD-cards. SD-card can be controlled by different interface types.
Namely SPI, SDIO. SDIO can work in 1 bit, 4 bit and 8 bit. In some MCUs there is a peripheral for SDIO
and you can take advantage of that fact using CubeMX.
For SPI, not using a predefined bord in CubeMX, you have to provide your own implementation.
You can find an SD-card based example for user_diskio.c in most Cube_FW... repositories.
For example STM32Cube_FW_F1_V1.4.0/Middlewares/Third_Party/FatFs/src/drivers/sd_diskio.c
There are functions in this file which are using IO functions like BSP_SD_ReadBlocks()
These functions in turn are using functions like
SD_IO_WriteReadData()
These functions in turn are using functions like
SPIx_WriteReadData()
These functions in turn are using functions like
HAL_SPI_TransmitReceive()
happy learning
Dieter
2017-02-26 1:14 PM
From :
STM32Cube\Repository\STM32Cube_FW_F1_V1.4.0\Middlewares\Third_Party\FatFs\src\drivers\sd_diskio.c
How can I link it with my generated code ? I don't understand ??
/**
****************************************************************************** * @file sd_diskio.c * @author MCD Application Team * @version V1.3.0 * @date 08-May-2015 * @brief SD Disk I/O driver ****************************************************************************** * @attention * * <h2><center>© COPYRIGHT 2015 STMicroelectronics</center></h2> * * Licensed under MCD-ST Liberty SW License Agreement V2, (the 'License'); * You may not use this file except in compliance with the License. * You may obtain a copy of the License at: **
* * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an 'AS IS' BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. * ****************************************************************************** *//* Includes ------------------------------------------------------------------*/
#include <string.h>#include 'ff_gen_drv.h'/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*//* Block Size in Bytes */#define BLOCK_SIZE 512/* Private variables ---------------------------------------------------------*/
/* Disk status */static volatile DSTATUS Stat = STA_NOINIT;/* Private function prototypes -----------------------------------------------*/
DSTATUS SD_initialize (BYTE);DSTATUS SD_status (BYTE);DRESULT SD_read (BYTE, BYTE*, DWORD, UINT);#if _USE_WRITE == 1 DRESULT SD_write (BYTE, const BYTE*, DWORD, UINT);#endif /* _USE_WRITE == 1 */#if _USE_IOCTL == 1 DRESULT SD_ioctl (BYTE, BYTE, void*);#endif /* _USE_IOCTL == 1 */ const Diskio_drvTypeDef SD_Driver ={ SD_initialize, SD_status, SD_read, #if _USE_WRITE == 1 SD_write,#endif /* _USE_WRITE == 1 */ #if _USE_IOCTL == 1 SD_ioctl,#endif /* _USE_IOCTL == 1 */};/* Private functions ---------------------------------------------------------*/
/**
* @brief Initializes a Drive * @param lun : not used * @retval DSTATUS: Operation status */DSTATUS SD_initialize(BYTE lun){ Stat = STA_NOINIT; /* Configure the uSD device */ if(BSP_SD_Init() == MSD_OK) { Stat &= ~STA_NOINIT; }return Stat;
}/**
* @brief Gets Disk Status * @param lun : not used * @retval DSTATUS: Operation status */DSTATUS SD_status(BYTE lun){ Stat = STA_NOINIT;if(BSP_SD_GetStatus() == MSD_OK)
{ Stat &= ~STA_NOINIT; } return Stat;}/**
* @brief Reads Sector(s) * @param lun : not used * @param *buff: Data buffer to store read data * @param sector: Sector address (LBA) * @param count: Number of sectors to read (1..128) * @retval DRESULT: Operation result */DRESULT SD_read(BYTE lun, BYTE *buff, DWORD sector, UINT count){ DRESULT res = RES_OK; if(BSP_SD_ReadBlocks((uint32_t*)buff, (uint64_t) (sector * BLOCK_SIZE), BLOCK_SIZE, count) != MSD_OK) { res = RES_ERROR; } return res;}/**
* @brief Writes Sector(s) * @param lun : not used * @param *buff: Data to be written * @param sector: Sector address (LBA) * @param count: Number of sectors to write (1..128) * @retval DRESULT: Operation result */#if _USE_WRITE == 1DRESULT SD_write(BYTE lun, const BYTE *buff, DWORD sector, UINT count){ DRESULT res = RES_OK; if(BSP_SD_WriteBlocks((uint32_t*)buff, (uint64_t)(sector * BLOCK_SIZE), BLOCK_SIZE, count) != MSD_OK) { res = RES_ERROR; } return res;}#endif /* _USE_WRITE == 1 *//**
* @brief I/O control operation * @param lun : not used * @param cmd: Control code * @param *buff: Buffer to send/receive control data * @retval DRESULT: Operation result */#if _USE_IOCTL == 1DRESULT SD_ioctl(BYTE lun, BYTE cmd, void *buff){ DRESULT res = RES_ERROR; SD_CardInfo CardInfo; if (Stat & STA_NOINIT) return RES_NOTRDY; switch (cmd) { /* Make sure that no pending write process */ case CTRL_SYNC : res = RES_OK; break; /* Get number of sectors on the disk (DWORD) */ case GET_SECTOR_COUNT : BSP_SD_GetCardInfo(&CardInfo); *(DWORD*)buff = CardInfo.CardCapacity / BLOCK_SIZE; res = RES_OK; break; /* Get R/W sector size (WORD) */ case GET_SECTOR_SIZE : *(WORD*)buff = BLOCK_SIZE; res = RES_OK; break; /* Get erase block size in unit of sector (DWORD) */ case GET_BLOCK_SIZE : *(DWORD*)buff = BLOCK_SIZE; break; default: res = RES_PARERR; } return res;}#endif /* _USE_IOCTL == 1 */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/2017-02-26 1:20 PM
Here's the complete generated code from STM32CubeMX, please have a look, thanks
https://drive.google.com/open?id=0B7YziG3F_7SqWklSdlZUSHN1dDQ
2017-02-26 2:41 PM
You have to know what pointers to functions are.
ff_gen_drv.h:
/**
* @brief Disk IO Driver structure definition
*/
typedef struct
{
DSTATUS (*disk_initialize) (BYTE); /*!< Initialize Disk Drive */
DSTATUS (*disk_status) (BYTE); /*!< Get Disk Status */
DRESULT (*disk_read) (BYTE, BYTE*, DWORD, UINT); /*!< Read Sector(s) */
#if _USE_WRITE == 1
DRESULT (*disk_write) (BYTE, const BYTE*, DWORD, UINT); /*!< Write Sector(s) when _USE_WRITE = 0 */
#endif /* _USE_WRITE == 1 */
#if _USE_IOCTL == 1
DRESULT (*disk_ioctl) (BYTE, BYTE, void*); /*!< I/O control operation when _USE_IOCTL = 1 */
#endif /* _USE_IOCTL == 1 */
}Diskio_drvTypeDef;
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Dieter
2017-02-27 12:08 AM
Hello Rick,
I have similar problem. The program stuck in fopen(). I posted a thread there:
https://community.st.com/0D50X00009XkfcxSAB
When I generate code using cubemx for F405, it works, but doesn't works for F4 The hardware problem was excluded because I have code generated by clive using spl. With that code, reading/writing has been passed.
I just couldn't figure out what is the problem.
2017-02-27 3:18 AM
In UM1721 page 19 :
3 FatFs applications
In the STM32CubeF4 solution, many applications are provided based on FatFsmiddleware. The table below gives you insight on how the FatFs middlewarecomponent is used in different examples which are classified by complexity anddepending on used physical drive interfaced (uSD, RAMDisk, USBDisk): ....
Where can I see those examples ? thanks
2017-02-27 3:27 AM
This is what I got :
STM32Cube\Repository\STM32Cube_FW_F1_V1.4.0\Projects\STM3210E_EVAL\Applications\FatFs
How can I adapt it to my custom code ?
2017-02-27 4:13 AM
Is there any working SDcard driver example ? I read from UM1718, there's an example ? where is it ?
It's not easy to write SDcard driver from scratch..