2016-03-24 04:22 PM
I upgraded to STM32CubeMX 4.14.0 and it tries to update STM32L4 FW to V1.4.0; at 39MB of the 224MB download it stops with a ''Problem during download'' error and if I try to download it at http://www.st.com/web/en/catalog/tools/PF261908, I can find only the V1.3.0 version. How can I update the STM32L4 package to the new version?
2016-03-24 05:39 PM
Will see if it downloads here. It could just be a connectivity issue, or one of free space.
The web download is actually 1.4.0, but the .ZIP is corrupted. [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/File%20STM32CubeL4.zip%20is%20currupted&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=14]See this thread2016-03-24 07:54 PM
Mirror of
https://drive.google.com/file/d/0B7OY5pub_GfIQXItZGRWRUZWa1k/view?usp=sharing
2016-03-25 09:19 AM
Would posting these ~200MB files as torrents be helpful to people?
The downloads took me an hour or more, on a high-bandwidth connection, and perhaps 5 minutes to push back onto the Google DriveThe packages can be pulled into CubeMX via ''From Local'' in the library manager.2016-03-25 12:01 PM
L4
/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_l4_vzip.torrent
/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_l4_vzip.torrent
F4/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_f4_vzip.torrent
________________ Attachments : stm32cube_fw_f4_v180.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpF&d=%2Fa%2F0X0000000aXK%2FdJYbZTdEpBwjk1aXqZZYbUkIYzThYVD1bsLhlKtoBS8&asPdf=falsestm32cube_fw_l4_v130.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpK&d=%2Fa%2F0X0000000aXL%2FW41lddJjgXmhM4Sn5cW9DpSnZcGtx.C.xNAK.MmkWh8&asPdf=falsestm32cube_fw_l4_v140.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpP&d=%2Fa%2F0X0000000aXN%2F1zgtYMbx_m6smC8nHLM44kKjBvoxNDkCM3YyCZLfFFg&asPdf=false2016-03-25 01:09 PM
Hi bancallari.luca,
It is fixed, now, in both website side and STM32CubeMx side. You can now easily update STM32CubeL4 in CubeMx to version 1.4.0. Also, you find the same 1.4.0 version ofhttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF261908
in our web side. Thank you for the feedbacks and sorry for this inconvenience from our side. -Hannibal-2016-03-25 01:36 PM
Many thanks!
2016-03-25 05:22 PM
Mirror of
https://drive.google.com/file/d/0B7OY5pub_GfINFJ6U3hpdklfV2c/view?usp=sharing