cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeL4 v1.4.0

Posted on March 25, 2016 at 00:22

I upgraded to STM32CubeMX 4.14.0 and it tries to update STM32L4 FW to V1.4.0; at 39MB of the 224MB download it stops with a ''Problem during download'' error and if I try to download it at http://www.st.com/web/en/catalog/tools/PF261908, I can find only the V1.3.0 version. How can I update the STM32L4 package to the new version?

7 REPLIES 7
Posted on March 25, 2016 at 01:39

Will see if it downloads here. It could just be a connectivity issue, or one of free space.

The web download is actually 1.4.0, but the .ZIP is corrupted. [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/File%20STM32CubeL4.zip%20is%20currupted&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=14]See this thread

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 25, 2016 at 03:54

Mirror of 

https://drive.google.com/file/d/0B7OY5pub_GfIQXItZGRWRUZWa1k/view?usp=sharing

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 25, 2016 at 17:19

Would posting these ~200MB files as torrents be helpful to people?

The downloads took me an hour or more, on a high-bandwidth connection, and perhaps 5 minutes to push back onto the Google Drive

The packages can be pulled into CubeMX via ''From Local'' in the library manager.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 25, 2016 at 20:01

L4

/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_l4_vzip.torrent

/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_l4_vzip.torrent

F4

/public/STe2ecommunities/mcu/Lists/STM32Java/Attachments/7494/stm32cube_fw_f4_vzip.torrent

________________

Attachments :

stm32cube_fw_f4_v180.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpF&d=%2Fa%2F0X0000000aXK%2FdJYbZTdEpBwjk1aXqZZYbUkIYzThYVD1bsLhlKtoBS8&asPdf=false

stm32cube_fw_l4_v130.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpK&d=%2Fa%2F0X0000000aXL%2FW41lddJjgXmhM4Sn5cW9DpSnZcGtx.C.xNAK.MmkWh8&asPdf=false

stm32cube_fw_l4_v140.zip.torrent : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpP&d=%2Fa%2F0X0000000aXN%2F1zgtYMbx_m6smC8nHLM44kKjBvoxNDkCM3YyCZLfFFg&asPdf=false
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Walid FTITI_O
Senior II
Posted on March 25, 2016 at 21:09

Hi bancallari.luca,

It is fixed, now, in both website side and STM32CubeMx side.

You can now easily update STM32CubeL4 in CubeMx to version 1.4.0.

Also, you find the same 1.4.0 version  of

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF261908

in our web side.

Thank you for the feedbacks and sorry for this inconvenience from our side.

-Hannibal-
Posted on March 25, 2016 at 21:36

Many thanks!

Posted on March 26, 2016 at 01:22

Mirror of

https://drive.google.com/file/d/0B7OY5pub_GfINFJ6U3hpdklfV2c/view?usp=sharing

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..