cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeL0 v1.5 does NOT contain low level API STM32l0xx_ll_.... files

Posted on April 26, 2016 at 08:50

Hi,

As per UM1749 User Manual  (Description of STM32L0 HAL and Low-layer drivers) the Low Level API should be found in:

''The Low Layer files are located in the same HAL drivers folder''

Figure 8: Low Layer driver folders''

Unfortunately there is no STM32l0xx_ll_.... files in this package.

Where can I find them?

Thanks,

Bogdan

1 ACCEPTED SOLUTION

Accepted Solutions
Walid FTITI_O
Senior II
Posted on May 25, 2016 at 12:10

Hi golab.bogdan,

 

Thr LL drivers are available now with STM32CubeL0 V1.6.0

-Hannibal-

View solution in original post

3 REPLIES 3
Posted on April 27, 2016 at 07:41

I verified that LL drivers are available in Cubex package for STML4. So it seems that in L0 package these LL drivers are missed (the supposed to be there in the L0 HAL & LL user guide).

Not sure where to report this issue.

Walid FTITI_O
Senior II
Posted on May 02, 2016 at 10:51

Hi golab.bogdan,

The Low Layer driver is not yet generated, that will be published on the web by end of the month. The document is update a little bit early. Sorry for the inconvenience.

-Hannibal-

Walid FTITI_O
Senior II
Posted on May 25, 2016 at 12:10

Hi golab.bogdan,

 

Thr LL drivers are available now with STM32CubeL0 V1.6.0

-Hannibal-