cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeL0 - USB example for STM32L073RZ

Marco Ferdinandi
Associate II
Posted on July 17, 2017 at 16:17

Hi,

I'm developing a bridge USB-SPI with a STM32L052 microcontroller. In this starting moment I'm developing the same application using the evaluation board STM32L073RZ. I'm using SW4STM32 IDE and STM32CubeL0 software. I'm looking for an example based on USB usage, but I haven't found yet.

Is there the USB driver for STM32L073RZ in the STM32CubeL0?

Are there any examples based on the USB?

Thanks in advance,

Marco Ferdinandi
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee
Posted on July 17, 2017 at 16:34

Hi

marco.ferdinandi@sensichips.com

‌,

Look to the ones available underSTM32Cube_FW_L0_V1.9.0\Projects\STM32L073Z_EVAL\Applications\USB_Device.

The device is the same (STM32L073), but you need to get rid of all BSP (board specific) code to run it in your own board.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Amel NASRI
ST Employee
Posted on July 17, 2017 at 16:34

Hi

marco.ferdinandi@sensichips.com

‌,

Look to the ones available underSTM32Cube_FW_L0_V1.9.0\Projects\STM32L073Z_EVAL\Applications\USB_Device.

The device is the same (STM32L073), but you need to get rid of all BSP (board specific) code to run it in your own board.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 17, 2017 at 16:58

Hi

st.mcu

,

thanks for the answer. I've Imported the STM32L073Z_EVAL project and I have built it successfully. Now, what should I do in order to customize this cose for my specific board (STM32L073RZ Nucleo)? What do you mean with 'to get rid of all BSP'? Should I replace something?

Thanks in advance.

Marco

Posted on July 17, 2017 at 17:23

The BSP code should be commented and the BSP related drivers have to be removed from the project to be used with the Nucleo.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Zt Liu
Senior III
Posted on July 18, 2017 at 05:58

hi, 

you may also consider to use cubeMX to generate the whole project, just enable USB FS and Enable Virtual Com Port 

stack. Then it' almost done!