cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeExpansion_MEMS1_V1.4.0 : *.ioc files

stephane239955
Associate II
Posted on November 30, 2015 at 08:57

Hello,

Starting a project based on datalog example delivered in this SW Package (STM32CubeExpansion_MEMS1_V1.4.0), I'm looking for an ioc file to initialize peripherals and cloks, but I'm unable to find it? Is-it hidden somewhere? Is there a way to rebuild it or create it quickly?

First trials doesn't works....

Any help gretaly appreciated

Best regards
1 REPLY 1
Nesrine M_O
Lead II
Posted on November 30, 2015 at 10:21

Hi Steph,

Unfortunately the software is not generated with CUBEMX, so the *ioc file for initialization code based on CubeMX is not included.

 

-Syrine-