cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32cube

Ahmetcancol
Associate

Hello, when I try to compile the code in the Stm32cubeide program, I see the error that the flash.ld file does not exist. And there is no file with flash.ld extension among my files. It is not created by stm32cubemx.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Ahmetcancol, to the community!
I am very sorry that this is happening to you. However, your information on this is quite sparse and so far we only know that the file is missing from your F1 project. It would at least make sense to upload the IOC file so that you can try to reproduce the problem.

In addition, the operating system and the versions of CubeMX and CubIDE you are using would also be useful to know.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.