cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cube mx

bob23
Associate II
Posted on October 13, 2014 at 14:58

I have installed STM32cubeMX and have some functionality. When I do a configuration and then try to generate code the cube window locks up. I left things for 40 minutes but no change.  A project file (.ioc ) is generated along with 2 small c files, but not the whole project. The target is MDK-ARM.

I have windows 7 professional 64 bit service pack 1, 8Gb ram, 8 core Intel(R) Core(TM) i7-4770 CPU @ 3.40GHz

Any ideas?
6 REPLIES 6
Posted on October 13, 2014 at 15:17

They'll ask you to attach the .IOC

What version of Java? What version of Keil? What board/chip?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bob23
Associate II
Posted on October 13, 2014 at 15:21

Thanks, clive1

java V7 update 67 (build 1.7.0_67-b01)

Ioc attached.

________________

Attachments :

f4_usb.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzSu&d=%2Fa%2F0X0000000bMA%2FwDCGfy4pswh5q70hnCX0eaUAJeKl_c36rC_x_EFRjLQ&asPdf=false
bob23
Associate II
Posted on October 13, 2014 at 15:26

MDK lite V5.11.1.0

STM32F4 discovery, with STM32F407VGT6

stm32cube-t
Senior III
Posted on October 14, 2014 at 16:56

Hello,

We do not reproduce your issue.

Can you please provide the .log file generated by MX in your user directory in .stm32cubemx folder

Can you also reproduce your error launching MX via the command line: java -jar STM32CubeMX.exe > output.log

Thanks

bob23
Associate II
Posted on October 15, 2014 at 08:58

Thanks for the reply. I zipped the whole project, I hope that you can find what you need.

Do you think it's worth a complete re-install?

Regards, Bob.

________________

Attachments :

f4_usb.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzSp&d=%2Fa%2F0X0000000bMB%2FjOk5XlWxpII7SKOCqQA_0KkDhkp8cTkke8vDF0HHwv0&asPdf=false
bob23
Associate II
Posted on October 20, 2014 at 10:56

Could this problem have anything to do with my tool chain  keil uv5 installation, it looks like the cube is expecting uv4 ?????

I can generate code if I select EWARM 6.7