cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube MX (STM32F407G) HAL + FreeRTOS

jose2
Associate
Posted on August 14, 2014 at 18:46

hi,

I'm novice with  STM32CubeMX   HAL + FreeRTOS    with  KEIL  MDK-ARM ulink2

I have problems, with SysTick probably, HAL_RCC_ClockConfig, because it genere HardFault_Handler.

When xPortSysTickHandler() in SysTickHandler() in ''stm32f4xx_it.c''  is in comment, there's  no hard fault... and without RTos , I have no problems.

Do you know the problem or do you have basic exemples for STM32F4xx HAL+FreeRTOS ?

merci

Jose Ferreira

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
jwoolston
Associate II
Posted on August 14, 2014 at 19:31

If you go to your user directory in Windows you should see a folder ''STM32Cube''. In there go to ''STM32Cube->Repository->STM32Cube_FW_F4_V1.3.0->Projects->STM324xG_EVAL->Applications->FreeRTOS''. It will have several examples for the OS. Additionally, other board demos exist that may be more specific to your needs.

rarthaud
Associate
Posted on August 18, 2014 at 09:07

Hello,

I had the same problem and traced it down to the priority group.

For some reason, it is set to NVIC_PRIORITYGROUP_0  with no way to change it in the GUI. This grouping only allows for subpriorities but no priority.

Forcing it to NVIC_PRIORITYGROUP_3 solves the problem.

Roland.

rarthaud
Associate
Posted on August 18, 2014 at 16:29

Actually, I meant NVIC_PRIORITYGROUP_4.

The priority group is global to the NVIC, but for some reason the generated code includes a HAL_NVIC_SetPriorityGrouping each time you have a peripheral requiring interrupts. And in my case, I don't know how I got the MX generator to have NVIC_PRIORITYGROUP_0 in my code, therefore preventing freeRTOS exception servicing.

jose2
Associate
Posted on August 19, 2014 at 11:49

Hi,

I solve the  problem by regenerating code with  STM32Cube MX  with theses changes in FreeRTOS config : 

USE_PREEMPTION  : disabled

USE_TRACE_FACILITY  : disabled

now it seems ok and I can discover my first RTOS...

Thanks to Roland and Jared

José

jarno
Associate III
Posted on August 19, 2014 at 12:44

once faced the same problem, read following thread for another solution: [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32CUBE%20%2b%20FreeRTOS%20%2b%20RTC%20HardFault&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21]STM32CUBE + FreeRTOS + RTC HardFault