STM32Cube Libraries PWM
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-19 4:38 AM
Posted on October 19, 2014 at 13:38
Hi, I am trying to output two PWM signals through channels 1 & 3 of TIM3.
I'm using the Nucleo F401RE board, so my MCU is STM32F401RE. I checked the example code included with the HAL and also the code generated by STM32CubeMX. This is my current code:#include ''stm32f4xx.h''
#include ''stm32f4xx_hal.h'' #include ''stm32f4xx_hal_rcc.h'' #include ''stm32f4xx_hal_gpio.h'' #include ''stm32f4xx_hal_tim.h'' #include ''stm32f4xx_hal_tim_ex.h'' #include ''uart.h'' #include ''xprintf.h'' TIM_HandleTypeDef htim3; intmain(
void)
{ UART_init(19200); xfunc_in = UART_getc; xfunc_out = UART_putc; xprintf( ''Initializing GPIO and Timer\n'');
GPIO_InitTypeDef GPIO_InitStruct; xprintf( ''1\n'');
/* Peripheral clock enable */ __GPIOC_CLK_ENABLE(); __TIM3_CLK_ENABLE(); xprintf( ''2\n'');
/**TIM3 GPIO Configuration PC6 ------> TIM3_CH1 PC8 ------> TIM3_CH3 */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF2_TIM3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); xprintf( ''3\n'');
TIM_ClockConfigTypeDef sClockSourceConfig; TIM_OC_InitTypeDef sConfigOC; TIM_MasterConfigTypeDef sMasterConfig; htim3.Instance = TIM3; htim3.Init.Prescaler = 35; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 100; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; HAL_TIM_Base_Init(&htim3); xprintf( ''4\n'');
HAL_TIM_PWM_Init(&htim3); xprintf( ''6\n'');
sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 25; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1); HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3); xprintf( ''7\n'');
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1); xprintf( ''8\n'');
inti = 0;
while(1)
{ __HAL_TIM_SetCompare(&htim3, TIM_CHANNEL_1, i++); if(i > 1700) i = 0;
HAL_Delay(100); } return0;
} When I launch the code it stops at the serial checkpoint number 6, so it seems to fail while configuring the PWM channel. When I pause the debug I notice that theHardFault_Handler(
void);
function is called. But if I remove the following line:HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);
it happens that the program reaches the checkpoint number 8 and enters the while loop, which makes no sense to me. Can someone help me? Thanks
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 2:22 AM
Posted on October 20, 2014 at 11:22
Hi Giacomo,
Are you facing an issue with HAL example as it is or problem is faced only after updating it?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-20 3:26 AM
Posted on October 20, 2014 at 12:26
Hi,
Can you attach your main.c file so that we can more easily figure out where a problem could be ?Regards,Heisenberg.