Skip to main content
Innomatic
Associate III
July 24, 2017
Question

STM32Cube L4 firmware v1.8.1 patch issue

Posted on July 24, 2017 at 05:43

STM32CubeMX v4.22 fails to merge L4 v1.8.1 patch with existing L4 v1.8.0 source tree. Instead it creates two distinctive trees, one for v1.8.0 and one for v1.8.1 when they are installed one after another, i.e. when you install v1.8.1 patch on top of existing v1.8.0 tree. Solution is to delete existing v1.8.0 repository entirely and install v1.8.1 from the scratch. I don't know it applies to other patches.

    This topic has been closed for replies.

    11 replies

    Khouloud GARSI
    ST Employee
    July 27, 2017
    Posted on July 27, 2017 at 12:58

    Hi

    Lee.Sungjune

    ‌,

    Thanks a lot for your feedback.

    The issue is internally forwarded to our CubeMX team.

    Khouloud.

    jeffl.kelley9
    Associate III
    August 29, 2017
    Posted on August 29, 2017 at 20:16

    Not interested in 'Patch' -- If version 1.8.1 exists, where do I download it from?

    Tesla DeLorean
    Guru
    August 29, 2017
    Posted on August 29, 2017 at 20:39

    I had CubeMX download them and merged the trees from the .ZIPs in the repository, want me to mirror that?

    I've argued multiple times that ST should provide a means to directly download these, or provide a torrent. This would increase the chance people could successfully download the files, and reduce the loading on the servers from recurrent and failing downloads of >600MB files.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jeffl.kelley9
    Associate III
    August 30, 2017
    Posted on August 30, 2017 at 17:09

    I'm good now, I just hand-merged the patch by assuming any files in it took precedence.